The M31/M33XXA Digitizers uses an internally generated high-quality clock (CLKref) which is phase-locked to the chassis clock. Therefore, this clock is an extremely jitter-cleaned copy of the chassis clock. This implementation achieves a jitter and phase noise above 100 Hz which is independent of the chassis clock, depending on it only for the frequency absolute precision and long term stability. A copy of CLKref is available at the CLK connector (Table 13).
CLKref is used as a reference to generate CLKsys, the high-frequency clock used to sample data.
| Programming Definitions | |||
|---|---|---|---|
|
Option |
Description |
Name |
Value |
|
Disable |
The CLK connector is disable
|
n/a |
0 (default) |
| CLKref Output | A copy of the reference clock is available at the CLK connector | n/a | 1 |
Table 13: M31/M33XXA Digitizers output clock configuration
The sampling frequency of the M31/M33XXA Digitizers (CLKsys frequency) can be changed using the advanced clocking system shown in Figure 7.
Figure 7: Functional diagram of the M31/M33XXA Digitizers FlexCLK system
where:
The CLKsys frequency can be changed within the range indicated in the datasheet of the corresponding product (function clockSet- Frequency, Section 2.3.4.17 on page 44). The CLKsync frequency changes with the CLKsys frequency as follows:
The CLKsync frequency is returned by the function clockSetFrequency
| Programming Definitions | |||
|---|---|---|---|
|
Option |
Description |
Name |
Value |
|
Low Jitter Mode |
The clock system is set to achieve the lowest jitter, sacrificing tuning speed |
CLK_LOW_JITTER |
0 |
|
Fast Tuning Mode |
The clock system is set to achieve the lowest tuning time, sacrificing jitter performance |
CLK_FAST_TUNE |
1 |
Table 14: Clock set frequency mode (function clockSetFrequency